Hi community,
I have some questions about i.MX6 LVDS spec.
[Q1]
Please see chapter 4.7.3 in IMX6DQCEC Rev.2.3.
There is "Operating Frequency" in Table 32, but there is not it in Figure 6.
So I want to confirm what is it.
I think it is a LVDS clock (LVDSx_CLK_x), is this correct?
[Q2]
Are there spec of "high levelo width" and "low level width" of LVDS clock?
[Q3]
There is no AC spec between LVDS clock and LVDS data.
Do you have it?
[Q4]
Do you have a spec about jitter of LVDS output?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
>[Q1]
Table 32 and Figure 6 describe all LVDS pads, this applicable to
LVDS clock (LVDSx_CLK_x) too.
[Q2],[Q3],[Q4]>
LVDS specifications use different timing concepts, than
"AC spec between LVDS clock and LVDS data" and
"high level width" and "low level width" of LVDS clock.
In particular EIA_644A standard [p.4] only requires that:
"The recommended signal transition time (tr, or tf) at the load should
not exceed 0.5 of the unit interval to preserve signal quality."
For LVDS timing requirements "eye pattern" analysis is used and based on
"eye pattern" test one can calculate allowable jitter, depending
on cable and its length. Please refer to app notes below and
other LVDS related app notes from other vendors.
National AN1088
https://archive.org/details/bitsavers_nationalap_130763
TI AN1059
http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=snla050&fileType=pdf
Maxim AN1856
>[Q1]
Table 32 and Figure 6 describe all LVDS pads, this applicable to
LVDS clock (LVDSx_CLK_x) too.
[Q2],[Q3],[Q4]>
LVDS specifications use different timing concepts, than
"AC spec between LVDS clock and LVDS data" and
"high level width" and "low level width" of LVDS clock.
In particular EIA_644A standard [p.4] only requires that:
"The recommended signal transition time (tr, or tf) at the load should
not exceed 0.5 of the unit interval to preserve signal quality."
For LVDS timing requirements "eye pattern" analysis is used and based on
"eye pattern" test one can calculate allowable jitter, depending
on cable and its length. Please refer to app notes below and
other LVDS related app notes from other vendors.
National AN1088
https://archive.org/details/bitsavers_nationalap_130763
TI AN1059
http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=snla050&fileType=pdf
Maxim AN1856