i.MX6 - Kernel changes for 2GB RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 - Kernel changes for 2GB RAM

533件の閲覧回数
Ansari
Contributor IV

Dear sir/Madam,

We are using i.MX6Q custom board based on sabreSD board and we are using Linux-3.10.17_1.0.0-GA BSP for our development.

We have upgraded the RAM size into 2GB (earlier it was 1GB).

We would like to know the changes required in u-boot and Kernel for 2GB with below BSPs.

1. Linux-3.10.17_1.0.0-GA

2. L3.0.35_4.1.0_130816

Regards,

Ansari

0 件の賞賛
1 返信

372件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to  Chapter 1 (Porting U-Boot from an i.MX 6 Reference

Board to an i.MX 6 Custom Board) of “i.MX_BSP_Porting_Guide.pdf” in

FSL Linux documentation.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛