Hi,
I have an issue where I can downsize a 2592x1944 image to 640x480 using the i.MX6 IPU successfully, but when I try other output resolutions (such as 1296x972) I get a garbaged picture.
In both cases the only thing that was changed in the code is the input width and height, but one case gives a correctly scaled image, while the other outputs garbage.
I'm running on Linux version 3.0.35-2026-geaaf30e.
I used mxc ipu unit test as a reference, and wrote this code: http://pastebin.com/pwF6dDcz
Compiled with: arm-fsl-linux-gnueabi-gcc (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) 4.6.2 20110630 (prerelease)
Tried it on 3.0.15 as well, it gives exactly the same results.
Any suggestions?
Solved! Go to Solution.
update from SR related:
Hi Jimmy,
There's no need to take this further, I've found in the IPU spec a restriction of the output image to 1024x1024.
update from SR related:
Hi Jimmy,
There's no need to take this further, I've found in the IPU spec a restriction of the output image to 1024x1024.