Hi,
I have a question of di0_sync_count_sel bit in IPUx_DI0_GENERAL register.
It described that 'For synchronous flow error: selects synchronous flow synchronization counter in DI:'
What is is this synchronization counter? Is it one of counter #0 to #8 in DI?
If so, How to chose the counter? IS it like, if DISP clock would like to stop, chose counter #0, or if Hsync would like to stop, chose counter#2?
Best Regards,
Sugiyama
Yes, the di0_sync_count_sel bit field selects between the DI counters #1 to #8.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, Artur,
Could you teach how counter # set?
Is it below case or another?
Case1:
0000 counter is disabled
0001 counter #1 is selected
1000 counter #8 is selected
Case2:
000 Counter is disabled
001 The counter is triggered by the same trigger that triggers the displays clock.
010 The Counter is triggered by counter #1
011 The Counter is triggered by counter #2
100 The Counter is triggered by counter #3
:
101 The Counter is triggered by counter #8
Best Regards,
Sugiyama
Hi, Artur,
Thank you for the answer.
I understood.
Best Regards,
Sugiyama
Hi, Artur,
Can you answer this counter # question?
Best Regards,
Sugiyama