Hi community,
I have a question about i.MX6 Series IPU.
Please see my question as below.
[Q1]
I think i.MX6 IPU CSI can capture even though input frame rate is over 60fps if it is less than 240MHz.
Is this correct?
(e.g. SVGA(800*600) * 120fps * 1.35 * 3cycles/pixel(RGB888) = 233MHz)
[Q2]
i.MX6 IPU DI can output over 60fps image to a display also if it is less than 240MHz.
Is this correct?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
Hi Satoshi
1. you are right
2. yes, for DI performance one can look at
p.14 IPU presentation
A Deep Dive into Image Processing for i.MX 6 Series Applications Processors
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
1. you are right
2. yes, for DI performance one can look at
p.14 IPU presentation
A Deep Dive into Image Processing for i.MX 6 Series Applications Processors
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------