i.MX6 IPU : When should "ext_vsync" be set in a proper value?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 IPU : When should "ext_vsync" be set in a proper value?

850 Views
norishinozaki
Contributor V

Hello Champs,

I'm looking at BSP 3.14.28_1.0.0 kernel source.

In a source file, mxc_v4l2_capture.c in drivers/media/platform/mxc/capture directory,

a function "mxc_v4l_open()" just sets 0 to "ext_vsnyc", but sets proper target values to Vsync_pol, Hsync_pol in line 1661 and 1662 like this.

        csi_param.Vsync_pol = ifparm.u.bt656.nobt_vs_inv;

        csi_param.Hsync_pol = ifparm.u.bt656.nobt_hs_inv;

On the other hand, "mxc_v4l2_s_param()" explicitly sets proper values for Vsync_pol, Hsync_pol and ext_vsync like this:

    csi_param.Vsync_pol = ifparm.u.bt656.nobt_vs_inv;

    csi_param.Hsync_pol = ifparm.u.bt656.nobt_hs_inv;

    csi_param.ext_vsync = ifparm.u.bt656.bt_sync_correct;

Is there any reason why "mxc_v4l_open()" doesn't set "ext_vsnyc" like above?

I just thought, all parameters should be properly set in "mxc_v4l_open()" without calling "mxc_v4l2_s_param()".

BR,

Nori Shinozaki

Labels (2)
0 Kudos
2 Replies

610 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Nori,

For the case of IPU, please check the ipu-csi.c driver file where the CSI bus config struct fill the ext_vsync accroding to v4l and mbus or csi usage. in case mxc_v4l_open you need to check and/or modify the static struct video_device mxc_v4l_template.

regards

0 Kudos

610 Views
norishinozaki
Contributor V

Hello,

Thanks but I can't find ipu-csi.c in the Linux kernels around 3.14.28.

Which version do you refer to?

BR,

Nori Shinozaki

0 Kudos