i.MX6 HDMI L-PCM support.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 HDMI L-PCM support.

ソリューションへジャンプ
1,104件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL HDMI.

I have understood i.MX6DL HDMI support 16, 24 bits L-PCM in https://community.freescale.com/thread/349086.

Then, please see chapter 13.2.5 in IMX6SDLLXRM Rev.Rev L3.0.35_4.1.0 (for L3.0.35_4.1.0_BSP).

24 bits audio is not mentioned in this chapter.

In addition, in sound/soc/imx/imx-hdmi-dma.c in L3.0.35_4.1.0, there is the following comment.

/* 24bit not support now. */

So we understood i.MX6SDL supports 24 bits L-PCM, but driver is not supported.

Is this correct?

Best Regards,

Satoshi Shimoda

ラベル(5)
タグ(2)
0 件の賞賛
返信
1 解決策
834件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

mx6 can support 24bits, different bsp version has different driver support. normally you can configure the asound.conf to support it.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
834件の閲覧回数
eric_kang
Contributor II

Dear All,

I have a same problem in the customer board.

I'm using the i.MX6Q / Linux 3.14.52

Could you tell me how to confirm the 24bit HDMI Audio on i.MX6 Evaluation board?

Best Regards,

Eric.

0 件の賞賛
返信
835件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

mx6 can support 24bits, different bsp version has different driver support. normally you can configure the asound.conf to support it.

0 件の賞賛
返信