Hi all,
I have a custom i.MX6 board and I want to use the CAN port.
I have a TJA1042 transceiver in normal mode (Standby wired to LOW not a GPIO control) [TJA1042 has 8 pins : CANH CANL TX(goes on TX i.mx6) RX(goes on RX i.mx6) VCC GND STB SPLIT/VIO]
I built an image with the can utils. I tested the can-bus with a can receiver and a can sender. My sender and receiver are tested, the receiver display what the sender "says".
When I activate the canbus on my board I got that :
root@imx6qsabresd:~# dmesg | grep CAN
vcan: Virtual CAN interface driver
CAN device driver interface
root@imx6qsabresd:~# dmesg | grep can
vcan: Virtual CAN interface driver
flexcan netdevice driver
flexcan imx6q-flexcan.1: device registered (reg_base=c09b8000, irq=143)
can: controller area network core (rev 20090105 abi 8)
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
//First method
root@imx6qsabresd:~# canconfig can0 bitrate 500000
can0 bitrate: 500000, sample-point: 0.866
root@imx6qsabresd:~# ifconfig can0 up
flexcan imx6q-flexcan.1: writing ctrl=0x03292005
//Second method
root@imx6qsabresd:~# ip link set can0 up type can bitrate 500000
flexcan imx6q-flexcan.1: writing ctrl=0x03292005
root@imx6qsabresd:~# ifconfig can0 up
root@imx6qsabresd:~# ifconfig
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
UP RUNNING NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:143
When I try to send a can message I got this
root@imx6qsabresd:~# cansend can0 500#1E.10.10
interface = can0, family = 29, type = 3, proto = 1
But nothing happen on the bus (receiver doesn't have any message and there is no activity on the oscilloscope on CANL/CANH or on TX line to transceiver)
When I repeat cansend about 12 times I finally got an error
root@imx6qsabresd:~# cansend can0 500#1E.10.10
interface = can0, family = 29, type = 3, proto = 1
write: No buffer space available
When I try to read a can message I got no activity whereas I see signal with oscilloscope on CANL CANH and RX line
root@imx6qsabresd:~# candump can0
interface = can0, family = 29, type = 3, proto = 1
I modifiy the kernel3.0.35-4.1.0/arch/arm/mach-mx6/board_myboard.c modifcations are inspired from sabrelite and sabreauto boards
static iomux_v3_cfg_t mx6q_etsjq7_pads[] = {
// ...
/* CAN1 */
MX6Q_PAD_GPIO_7__CAN1_TXCAN,
MX6Q_PAD_GPIO_8__CAN1_RXCAN,
//...
};
static void mx6q_etsjq7_flexcan1_switch(int enable)
{
}
static const struct flexcan_platform_data
mx6q_etsjq7_flexcan1_pdata __initconst = {
.transceiver_switch = mx6q_etsjq7_flexcan1_switch,
};
imx6q_add_flexcan1(&mx6q_etsjq7_flexcan1_pdata);
解決済! 解決策の投稿を見る。
Hi,
Problem solved.
To build my kernel I followed this DOC
but I made a mistake because I have to init flexcan0 and not flexcan1.
HI:
timl,Can you give me some advise here:https://community.nxp.com/thread/437311
HI
timl,I've come across this problem.Can you give me some advise.
Hi,
Problem solved.
To build my kernel I followed this DOC
but I made a mistake because I have to init flexcan0 and not flexcan1.
Access Denied
You don't have permission to access "http://www.nxp.com=ns-404=docs=DOC-94887" on this server.
Reference #18.ae0ae07a.1627451656.2c36f3f0
Access Denied
You don't have permission to access "http://www.nxp.com\/ns-404\/docs\/DOC-94887" on this server.
Reference #18.ae0ae07a.1627451656.2c36f3f0
Hi,
Have you checked this? I believe it can be very useful to realize the needed changes.
https://community.freescale.com/message/302837#302837
Regards,
Alejandro