i.MX6 ENET MAC output in sleep mode.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 ENET MAC output in sleep mode.

ソリューションへジャンプ
1,242件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 ENET.

Please see chapter 23.6.7.1 in IMX6SDLRM Rev.2.

It says that "The transmit logic is disabled." in sleep mode.

We think this means "i.MX6 output Hi-Z in sleep mode, is this understanding correct?

Best Regards,

Satoshi Shimoda

タグ(1)
0 件の賞賛
返信
1 解決策
1,181件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The sleep mode, mentioned in section 23.6.7.1 (Sleep mode), relates to

the internal MAC module only, it does not affect external pins.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,182件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The sleep mode, mentioned in section 23.6.7.1 (Sleep mode), relates to

the internal MAC module only, it does not affect external pins.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信