i.MX6 EIM burst access and WC bit setting.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 EIM burst access and WC bit setting.

Jump to solution
1,774 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6SDL EIM.

Please see chapter 22.9.1 in IMC6SDLRM (Rev.1).

I want to know what is different between the following two cases.

[Case 1]

WC: 0 (Write access burst length occurs according to BL value)

BL: 100 (Continuous burst length)

SWR: 1 (write accesses are in Synchronous mode)

[Case 2]

WC: 1 (Write access burst length is continuous)

SWR: 1 (write accesses are in Synchronous mode)

Would you let me know what is different and what defines the burst length in each case?

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (1)
1 Solution
1,538 Views
art
NXP Employee
NXP Employee

Generally, there is no difference between these two cases.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,539 Views
art
NXP Employee
NXP Employee

Generally, there is no difference between these two cases.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,538 Views
satoshishimoda
Senior Contributor I

Hi community,

Would you give me advice?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply