i.MX6 EIM 8 bit port.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 EIM 8 bit port.

跳至解决方案
1,411 次查看
satoshishimoda
Senior Contributor I

Hi, communty,

A customer has some questions about i.MX6SDL EIM.

[Q1]

Please see the description of DSZ field in chapter 22.9.1 of IMX6SDLRM Rev.1.

It says "NOTE: Only async. access supported for 8 bit port.".

Customer is confused this expression.

Which is correct?

1. Async access can use only 8 bit port. (cannot use 16 bit port & 32 bit port)

2. Only async access can use 8 bit port. (sync access cannot use 8 bit port)

I guess 2. is correct, right?

[Q2]

Please see chapter 22.5.3.

It says "All modes are supported in with 8-, 16- or 32-bit port configuration, according to DSZ bit field".

But 8 bit port configuration is limited according to DSZ bit field.

Is this right?

Best Regards,

Satoshi Shimoda

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
1,135 次查看
Yuri
NXP Employee
NXP Employee

Briefly :


1.
Correct, only async access can use 8 bit port (sync access cannot use 8 bit port).

2.
This is inaccuracy in Chapter 22.5.3, really "8 bit port configuration is limited" and
"sync access cannot use 8 bit port".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,136 次查看
Yuri
NXP Employee
NXP Employee

Briefly :


1.
Correct, only async access can use 8 bit port (sync access cannot use 8 bit port).

2.
This is inaccuracy in Chapter 22.5.3, really "8 bit port configuration is limited" and
"sync access cannot use 8 bit port".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复