i.MX6 EIM 8 bit port.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 EIM 8 bit port.

Jump to solution
783 Views
satoshishimoda
Senior Contributor I

Hi, communty,

A customer has some questions about i.MX6SDL EIM.

[Q1]

Please see the description of DSZ field in chapter 22.9.1 of IMX6SDLRM Rev.1.

It says "NOTE: Only async. access supported for 8 bit port.".

Customer is confused this expression.

Which is correct?

1. Async access can use only 8 bit port. (cannot use 16 bit port & 32 bit port)

2. Only async access can use 8 bit port. (sync access cannot use 8 bit port)

I guess 2. is correct, right?

[Q2]

Please see chapter 22.5.3.

It says "All modes are supported in with 8-, 16- or 32-bit port configuration, according to DSZ bit field".

But 8 bit port configuration is limited according to DSZ bit field.

Is this right?

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
1 Solution
507 Views
Yuri
NXP Employee
NXP Employee

Briefly :


1.
Correct, only async access can use 8 bit port (sync access cannot use 8 bit port).

2.
This is inaccuracy in Chapter 22.5.3, really "8 bit port configuration is limited" and
"sync access cannot use 8 bit port".

Have a great day,
Yuri
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
508 Views
Yuri
NXP Employee
NXP Employee

Briefly :


1.
Correct, only async access can use 8 bit port (sync access cannot use 8 bit port).

2.
This is inaccuracy in Chapter 22.5.3, really "8 bit port configuration is limited" and
"sync access cannot use 8 bit port".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos