[i.MX6] Does DDR parameters need to fill into uboot and kernel on Yocto 3.14.52_1.1.0 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[i.MX6] Does DDR parameters need to fill into uboot and kernel on Yocto 3.14.52_1.1.0 ?

826 Views
charleshuang
Senior Contributor II

In order to stabilize the system, does DDR parameters need to fill into uboot and kernel?

Thank you.

Best Regards,

Alex

0 Kudos
Reply
1 Reply

712 Views
igorpadykov
NXP Employee
NXP Employee

Hi charles

after running ddr tester new calibration settings should be added

manually to *.cfg file like uboot/board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply