i.MX6 DL/S Android JB4.2.2_1.0.0-GA release

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 DL/S Android JB4.2.2_1.0.0-GA release

2,347 Views
sachusanal
Contributor III

Hi sir ,

I need Prebuilt android OS image for IMX6qsabresd  please share me the link

through this link i.MX6 D/Q and i.MX6 DL/S Android JB4.2.2_1.0.0-GA release i try to download source code but source code is not availble please help me

Labels (1)
6 Replies

1,680 Views
Yuri
NXP Employee
NXP Employee

  Please send me Your e-mail, so that I can forward You link to load the package from archive.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,680 Views
justinliao
Contributor I

Hi, Yuri

I also need that version of for customer project debug.

My mail is justin.liao@amod.com.tw

Thanks for your help.

0 Kudos
Reply

1,680 Views
sachusanal
Contributor III
0 Kudos
Reply

1,680 Views
sachusanal
Contributor III

Thanks for your response

Mail Id: sachu.sanal@nestgroup.net

please give source code and Documents

Board:IMX6QSabresd board development Kit which is purchased from freescale

0 Kudos
Reply

1,680 Views
saurabh206
Senior Contributor III

Android 4.2.2.1.1 is no longer maintained by Freescale but you can download newer versions of android from the following link:

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

1,680 Views
sachusanal
Contributor III

Hi ,

Thanks for your response .

could you please  tell me the exact location  under run time softwares /operating system support board support packages

0 Kudos
Reply