i.MX6 DISP0, DISP1 Parallel Video HSYNC, VSYNC, etc.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 DISP0, DISP1 Parallel Video HSYNC, VSYNC, etc.

891 Views
stephenbarton
Contributor II

We are designing an iMX6 Dual system using both parallel DISP Video Outputs.

In the "i.MX 6Dual/6Quad Applications Processor Reference Manual, Rev. 3, 07/2015",

"Table 37-6. IPU1 External Signals" suggests that IPU1 can drive both the DISP0 outputs and the DISP1 outputs (on the EIM pads)

"Table 37-7. IPU2 External Signals"  suggests that IPU2 can drive the DISP0 outputs only - not the DISP1 outputs.

In other words, both IPU's can drive DISP0;  only IPU1 can drive DISP1.

Is this info correct?

It is not clear from the Reference Manual which 8 pads to use for the pixel CLK, HSYNC, VSYNC and Data Enable outputs on these DISP0 and DISP1 ports?

Are these 8 pads documented somewhere?

Thanks

- Stephen

Labels (2)
0 Kudos
1 Reply

420 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please use Figure 9-2 (Display port muxing scheme) of the i.MX6 RM.

 

http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6DQRM.pdf 

 

  Also, please refer to section 4.11.10.4 (IPU Display Interface Signal Mapping)

of the i.MX6 Datasheet.

http://www.nxp.com/assets/documents/data/en/data-sheets/IMX6DQCEC.pdf 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you

0 Kudos