i.MX6 DDR Stress Test Tool V1.0.3.1 for LPDDR2 4K interleaved mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 DDR Stress Test Tool V1.0.3.1 for LPDDR2 4K interleaved mode

6,284件の閲覧回数
GraceH
Senior Contributor II

Version V1.0.3.1 is only for i.MX6Q/6D LPDDR2 4K interleaved mode.

For other configuration, please use i.MX6 DDR Stress Test Tool V1.0.3

Original Attachment has been moved to: DDR_Stress_Tester_V1.0.3.1_LPDDR2_interleaved.zip

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

1,843件の閲覧回数
XiaoPong
NXP Employee
NXP Employee

Hi, Grace,

     Met unauthorized error when accessing the doc of i.MX6 DDR Stress Test Tool V1.0.3 from your link.

0 件の賞賛
返信

1,843件の閲覧回数
GraceH
Senior Contributor II

It seems community upgrade causes problem. A lots of posts disappeared.

Please wait.

Grace

0 件の賞賛
返信

1,843件の閲覧回数
anrov
Contributor I

When DDR_Stress_Test.exe (v1.0.3.1 interleaved) prompts:

     "Please select the DDR density of two channels(in bytes) on the board"

what option do I choose for a 2GByte package (MT42L256M64D4LM-25)?

I've been choosing "0 for 2GB".

The manual for v1.0.2 only shows a screenshot with the prompt:

     "Please select the DDR density per CHANNEL(in bytes) on the board"

0 件の賞賛
返信