i.MX6 DCIC freeze

cancel
Showing results for 
Search instead for 
Did you mean: 

i.MX6 DCIC freeze

968 Views
marioschuknecht
Contributor I

We use DCIC in our system. Sometimes the system freezes.
We use kernel 4.1.15, Yocto as build environment, and the device tree is configured as follows:

dcic1: dcic@020e4000 {
   compatible = "fsl,imx6q-dcic";
   reg = <0x020e4000 0x4000>;
   interrupts = <0 124 IRQ_TYPE_LEVEL_HIGH>;
   clocks = <&clks IMX6QDL_CLK_DCIC1>, <&clks IMX6QDL_CLK_DCIC1>;
   clock-names = "dcic", "disp-axi";
   gpr = <&gpr>;
   status = "disabled";
};

&dcic1 {
   dcic_id = <0>;
   dcic_mux = "dcic-lvds0";
   status = "okay";
};

The demo program mxc_dcic_test.out from the imx-test package works without problems. 

I can create a similar behavior when the line 
      Ioctl (fd_fb0, FBIOBLANK, FB_BLANK_UNBLANK);

is removed in the main function from mxc_dcic_test.c.

echo 1 > /sys/class/graphics/fb0/blank
and
mxc_dcic_test.out -dev 0
cause the system to freeze immediately.

Has anyone observed this behavior? Or can give hints how I can find the error?

Labels (4)
Tags (2)
0 Kudos
3 Replies

474 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Mario

seems it freezes as fb is turned off with command

force enter in the fb sleep mode
echo 1 >/sys/class/graphics/fb0/blank     # off 

to disable lcd turning off one can check

https://community.nxp.com/thread/323250

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

474 Views
marioschuknecht
Contributor I

Hi Igor,

You're right. It seems that something turns off fb0 during boot.

If I unblank fb0 each time before call of DCIC-ioctl in my loop, the system does not freeze.

while (1)

{

    ioctl(fd_fb0, FBIOBLANK, FB_BLANK_UNBLANK);

    ioctl(fd_dcic, DCIC_IOC_GET_RESULT, &result);

    ....

}

Regards

Mario

0 Kudos

474 Views
marioschuknecht
Contributor I

Hi Igor,

Interesting hint and link. The vt.c driver is enabled in my kernel. I've checked your note and add "consoleblank=0" to kernel bootargs.

The problem still exists.

If the error occurs, it always occurs when booting. A systemd service starts my unit and then it comes to the error.

Mario

0 Kudos