i.MX6 Carplay (3.10.17)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 Carplay (3.10.17)

跳至解决方案
3,948 次查看
brucecollie
Contributor I

Hi,

I am currently working on implementing Apple's Carplay software on an i.MX6 board. This requires USB OTG role swapping, which is not included in the supported BSP I am using:

Board: imx6qsabreauto

BSP: 3.10.17

This functionality is implemented in version 3.17 of the kernel, and this thread suggests that a patch exists to include the functionality in 3.10.17.

Is there any way to build 3.17 for the device, or can anyone point me in the right direction to obtain a patch for 3.10.17?

Thank you

0 项奖励
回复
1 解答
2,599 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Bruce,

I got the patch and I also realized that Yong posted it on the referenced thread. You can find the patch here:

https://community.freescale.com/thread/351582#528873


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,598 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Bruce,

I have asked for the patch. I will post an update as soon as having news.

Best regards!

/Carlos

0 项奖励
回复
2,600 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Bruce,

I got the patch and I also realized that Yong posted it on the referenced thread. You can find the patch here:

https://community.freescale.com/thread/351582#528873


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,599 次查看
brucecollie
Contributor I

Hi Carlos,

Would you be able to let me know the licensing situation with the supplied patch? We would like to be able to distribute the code as part of our product if possible.

Thanks

0 项奖励
回复
2,599 次查看
brucecollie
Contributor I

Hi Carlos,

I did indeed receive the patch from Yong. I am happy to report that it works as intended.

Thanks for all your help,

Bruce

0 项奖励
回复