Hi community,
I have a question about i.MX6SDL CSI2IPU.
Please see chapter 19.1.1 in IMX6DQRM, I want to confirm about " Dynamically configurable RGB444 and YUV422 data format for the IPU module".
I understand this is usable to adjust data alignment only when input data format is RGB444 or YUV422, so RGB444_FM bit and YUV422_8bit_FM bit in CSI2IPU_SW_RST register setting are "Dont' care" if other format is input.
Is my understanding correct?
Best Regards,
Satoshi Shimoda
Hi Satoshi
yes this understanding is correct.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------