i.MX6 CSI -> VDIC path

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 CSI -> VDIC path

Jump to solution
1,491 Views
satoshishimoda
Senior Contributor I

Hi all,

We want to use de-interlacing for the image from CSI as attached path.

Then, we think we have to set VDI_SRC_SEL field to 01b (CSI direct(cb7)) in chapter 37.5.34 in IMX6DQRM (Rev.1) for using the attached path, isn't it?

On the other hand, there is no setting to set CSI destination = VDIC in CSI0_DATA_DEST field in chapter 37.5.152.

What value should we set to CSI0_DATA_DEST in this case?

And if more setting is needed to use the attached de-interlacing path, could you let us know also?

Best Regards,

Satoshi Shimoda

Labels (5)
0 Kudos
1 Solution
710 Views
Yuri
NXP Employee
NXP Employee

The VDI_SRC_SEL should be set as 01b (CSI direct(cb7)).

The CSI0_DATA_DEST should be set as CSI0_DATA_DEST[2] - destination is IDMAC via SMFC.

View solution in original post

0 Kudos
2 Replies
711 Views
Yuri
NXP Employee
NXP Employee

The VDI_SRC_SEL should be set as 01b (CSI direct(cb7)).

The CSI0_DATA_DEST should be set as CSI0_DATA_DEST[2] - destination is IDMAC via SMFC.

0 Kudos
710 Views
satoshishimoda
Senior Contributor I

Anybody can reply?

In fact, our dead line is close, so I appreciate if you give me a reply soon.

Best Regards,

Satoshi Shimoda

0 Kudos