i.MX6 CSI -> VDIC path

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 CSI -> VDIC path

跳至解决方案
1,532 次查看
satoshishimoda
Senior Contributor I

Hi all,

We want to use de-interlacing for the image from CSI as attached path.

Then, we think we have to set VDI_SRC_SEL field to 01b (CSI direct(cb7)) in chapter 37.5.34 in IMX6DQRM (Rev.1) for using the attached path, isn't it?

On the other hand, there is no setting to set CSI destination = VDIC in CSI0_DATA_DEST field in chapter 37.5.152.

What value should we set to CSI0_DATA_DEST in this case?

And if more setting is needed to use the attached de-interlacing path, could you let us know also?

Best Regards,

Satoshi Shimoda

标签 (5)
标记 (4)
0 项奖励
1 解答
751 次查看
Yuri
NXP Employee
NXP Employee

The VDI_SRC_SEL should be set as 01b (CSI direct(cb7)).

The CSI0_DATA_DEST should be set as CSI0_DATA_DEST[2] - destination is IDMAC via SMFC.

在原帖中查看解决方案

0 项奖励
2 回复数
752 次查看
Yuri
NXP Employee
NXP Employee

The VDI_SRC_SEL should be set as 01b (CSI direct(cb7)).

The CSI0_DATA_DEST should be set as CSI0_DATA_DEST[2] - destination is IDMAC via SMFC.

0 项奖励
751 次查看
satoshishimoda
Senior Contributor I

Anybody can reply?

In fact, our dead line is close, so I appreciate if you give me a reply soon.

Best Regards,

Satoshi Shimoda

0 项奖励