Hi all,
We want to use de-interlacing for the image from CSI as attached path.
Then, we think we have to set VDI_SRC_SEL field to 01b (CSI direct(cb7)) in chapter 37.5.34 in IMX6DQRM (Rev.1) for using the attached path, isn't it?
On the other hand, there is no setting to set CSI destination = VDIC in CSI0_DATA_DEST field in chapter 37.5.152.
What value should we set to CSI0_DATA_DEST in this case?
And if more setting is needed to use the attached de-interlacing path, could you let us know also?
Best Regards,
Satoshi Shimoda
解決済! 解決策の投稿を見る。
The VDI_SRC_SEL should be set as 01b (CSI direct(cb7)).
The CSI0_DATA_DEST should be set as CSI0_DATA_DEST[2] - destination is IDMAC via SMFC.
The VDI_SRC_SEL should be set as 01b (CSI direct(cb7)).
The CSI0_DATA_DEST should be set as CSI0_DATA_DEST[2] - destination is IDMAC via SMFC.
Anybody can reply?
In fact, our dead line is close, so I appreciate if you give me a reply soon.
Best Regards,
Satoshi Shimoda