Hi community,
Our partner have a question about i.MX6 Linux BSP thermal driver.
Please see chapter 26.1 in i.MX 6 Linux Reference Manual (IMX6LXRM Rev L3.10.17-1.0.0-ga) in Yocto BSP.
It says " When reaching passive point, cooling device will lower CPU frequency and notify GPU to run at a lower frequency."
Then, could you let me know the concrete frequency when the cooling?
(e.g. CPU = xxx MHz, GPU = yyy MHz)
Best Regards,
Satoshi Shimoda
Hi Satoshi
these frequencies are described in
"Software Thermal Driver" AN4579
i.MX 6 Series Thermal Management Guidelines
L3.10.17-1.0.0 setings basically the same and one can verify them
checking sources, mentioned in IMX6LXRM Rev L3.10.17-1.0.0-ga sect.26.3.1 Source Code Structure
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------