i.MX6 BT_CFG from GPIO not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 BT_CFG from GPIO not working

1,076 Views
jaydcarlson
Contributor III

I have a custom i.MX6-based design I'm bringing up with both MicroSD (on SDHC3) and eMMC (on SDHC1). I'm trying to boot from MicroSD right now. I've broken out the BT_CFG pins, and I'd like to set the boot config using GPIO pins.

Unfortunately, the i.MX6 always jumps to the USB serial download, no matter what settings I use on the BOOT_MODE[1:0] pins or the GPIO BT_CFG pins.

I've verified the correct voltages at the DIP switch used to set the boot mode, and I've tried it both from a cold boot, and by resetting the i.MX6 by pulling POR low -- either way, it jumps straight to USB serial download. I've verified the MicroSD card has a boot image that my RIoTBoard has no problems booting from.

Any ideas?

Here's my schematic:

LaJLhkV.png

Labels (3)
0 Kudos
3 Replies

697 Views
vacer-chen
Contributor I

I met the same problem :smileysad: , can you tell me the solution ??

0 Kudos

697 Views
Yuri
NXP Employee
NXP Employee

Hello,

1.

  Please check SRC_SBMR1 register of the i.MX6 (with a JTAG debugger)

“The Boot Mode register (SBMR) contains bits that reflect the status of Boot
Mode Pins of the chip.”

2.
Please verify if any SD accesses are provided during boot.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

697 Views
jaydcarlson
Contributor III

1. SRC_SBMR1 has a value of 0x3040. BOOT_CFG1 = 0x40 indicates that SD/eSD is selected (with all default options: regular boot, normal SD speed, no power cycle, and internal loopback clock source). Boot_CFG2 = 0x30 indicates all default options other than enabling 4-bit bus width

2. I put a scope probe on the SD_CMD pin, and it wiggles around a bit when power is applied.

After looking at the suggested signals, it looks like it's trying to boot from MicroSD card, but can't?

I'm looking at hardware issues:

I didn't put any pull-up resistors on the SD card's pins, as I thought I read somewhere they were internally pulled-up. Is this not true?

I only have 1 uF of decoupling on the SD card connector. I bumped it up to 22 uF by hanging a thru-hole electrolytic off the board by the connector, and that didn't change anything. Not sure if I need more.

Thanks!

0 Kudos