i.MX6 BSP for u-buntu 14.04 and linux 3.10.17

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 BSP for u-buntu 14.04 and linux 3.10.17

1,527 Views
misbahk
Contributor I

Hi All,

Where can download the stable release of i.MX6 BSP for ubuntu version 14.04 and linux kernel 3.10.17 ?

I have a yocto project for fsl-release-bsp, How can use the same for ubuntu 14.04 and linux 3.10.17 git download and build.

I need to use the yocto project from freescale for the development, please suggest.

--- Misbah

0 Kudos
Reply
1 Reply

881 Views
igorpadykov
NXP Employee
NXP Employee

Hi Misbah

i.MX6 BSP kernel 3.10.17 can be found on

Board Support Packages (29)

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo

Files and Linux BSP Documentation (REV L3.10.17_1.0.2)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply