i.MX6 BSP for u-buntu 14.04 and linux 3.10.17

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 BSP for u-buntu 14.04 and linux 3.10.17

1,491件の閲覧回数
misbahk
Contributor I

Hi All,

Where can download the stable release of i.MX6 BSP for ubuntu version 14.04 and linux kernel 3.10.17 ?

I have a yocto project for fsl-release-bsp, How can use the same for ubuntu 14.04 and linux 3.10.17 git download and build.

I need to use the yocto project from freescale for the development, please suggest.

--- Misbah

0 件の賞賛
返信
1 返信

845件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Misbah

i.MX6 BSP kernel 3.10.17 can be found on

Board Support Packages (29)

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo

Files and Linux BSP Documentation (REV L3.10.17_1.0.2)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信