According to the I.MX6S & i.MX6QP datasheets, the GPIO pins threshold levels are defined as:
Parameter | Symbol | Test Conditions | Min | Max | Units |
---|---|---|---|---|---|
High-Level input voltage | VIH | — | 0.7 × OVDD | OVDD | V |
Low-Level input voltage | VIL | — | 0 | 0.3 × OVDD | V |
Does this also apply to the levels of BOOT_MODE pins with OVDD beeing VDD_SNVS_IN?
If not - which thresholds have to be applied?
Thanks
KST
Hi Klaus
yes this also apply to the levels of BOOT_MODE pins with OVDD beeing VDD_SNVS_IN.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------