i.MX6 ARM cores rarely dead locked when communicated with ttymxc0.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 ARM cores rarely dead locked when communicated with ttymxc0.

730件の閲覧回数
torus1000
Contributor V

Hi,

Two ARM cores dead locked during test command input from console continuously.
It happened once per 24 hours. If dead lock happened, watchdog issue the reset.


Have anyone heard of this phenomenon?


What are the possible causes?

Our board info are as following.

kernel: L3.14.38
Board: Prototype board
host OS: Ubuntu14.04 Lemix(linaro14.04)
Serial port: port1(ttymxc0) 115200bps

Anyone can help me?

Thanks

ラベル(3)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

598件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Torus,

Did you check this Errata of the device

https://community.nxp.com/message/397208?commentID=397208#comment-397208 

All the ARM errata has been defined in the arch/arm/Kconfig, you can search from the file arch/arm/Kconfig.

 

If you want to see which ERRATA enabled on the i.MX6X, please check the .config file after running the build command: ‘make imx6_defconfig ARCH=ARM ….’

Jaime

0 件の賞賛
返信

598件の閲覧回数
torus1000
Contributor V

Hi Jaime,

I opened new case #00109023 and uploaded register value and system.map.
If you mind, would you reply above case?

Torus

0 件の賞賛
返信

598件の閲覧回数
torus1000
Contributor V

Hi Jaime,

I'm sorry the links you provide give me an error

Unauthorized
This place or content does not exist or access to it is restricted.

Is there any reachable links?

Torus

0 件の賞賛
返信