Hi all,
a newbie here!
I'm trying to implement a USB gadget device with my i.MX53QSB using High-Bandwidth USB isochronous transfers (3 packets/microframe) but, unfortunatelly, with NO success. If I use 1 packet/microframe I have no problem at all, it works flawlesslly. The BSP is L2.6.35_11.01.00 from Freescale.
To change from 1 packet to 3 packets/microframe operation, as far as I know, I only need to change the .wMaxPacketSize field of the endpoint descriptor, so:
- for 1 packet/microframe: .wMaxPacketSize = cpu_to_le16(0x0000+1024)
- for 3 packets/microframe: .wMaxPacketSize = cpu_to_le16(0x1000+1024)
Doing this, if I plug the QSB to my host machine (Ubuntu 11.04), I can see the following (lsusb -v):
- for 1 packet/microframe:
..... . .
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x82 EP 2 IN
bmAttributes 1
Transfer Type Isochronous
Synch Type None
Usage Type Data
wMaxPacketSize 0x0400 1x 1024 bytes
bInterval 1
..... . .
- for 3 packet/microframe:
..... . .
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x82 EP 2 IN
bmAttributes 1
Transfer Type Isochronous
Synch Type None
Usage Type Data
wMaxPacketSize 0x1400 3x 1024 bytes
bInterval 1
..... . .
so this looks OK.
The problem appears in "static int process_ep_req()" (in arcotg_udc.c), where "curr_td->size_ioc_sts" is always set to 0x8408 reporting a "DTD_STATUS_TRANSACTION_ERR" error. This only (and always) happens with 3 packets/microframe, no problem with 1 packet/microframe.
In /proc/driver/fsl_usb2_udc I'm not able to see any problem:
- for 1 packet/microframe:
root@freescale ~$ cat /proc/driver/fsl_usb2_udc
ARC USBOTG Device Controller driver
fsl-usb2-udc version: 1 August 2005
Gadget driver: g_webcam
USBCMD reg:
SetupTW: 0
Run/Stop: Run
USB Status Reg:
Dr Suspend: 0Reset Received: 0System Error: NormalUSB Error Interrupt: No err
USB Intrrupt Enable Reg:
Sleep Enable: 1SOF Received Enable: 0Reset Enable: 1
System Error Enable: 1Port Change Dectected Enable: 1
USB Error Intr Enable: 1USB Intr Enable: 1
USB Frame Index Reg:Frame Number is 0x1b89
USB Device Address Reg:Device Addr is 0x18000000
USB Endpoint List Address Reg:Device Addr is 0xcf3c6000
USB Port Status&Control Reg:
Port Transceiver Type : UTMIPort Speed: High Speed
PHY Low Power Suspend: Low power modePort Reset: Not in ResetPort Suspend Mode: Not in
Over-current Change: NoPort Enable/Disable Change: Not change
Port Enabled/Disabled: EnableCurrent Connect Status: Attached
USB Mode Reg:Controller Mode is : Device Controller
Endpoint Setup Status Reg:SETUP on ep 0x0
EP Ctrl Reg [0x0]: = [0x800080]
EP Ctrl Reg [0x1]: = [0x0]
EP Ctrl Reg [0x2]: = [0x840000]
EP Ctrl Reg [0x3]: = [0x0]
EP Ctrl Reg [0x4]: = [0x0]
EP Ctrl Reg [0x5]: = [0x0]
EP Ctrl Reg [0x6]: = [0x0]
EP Ctrl Reg [0x7]: = [0x0]
EP Prime Reg = [0x0]
For ep0 Maxpkt is 0x40 index is 0x0
req df582b40 actual 0x1a length 0x1a buf df485500
For ep2in Maxpkt is 0x400 index is 0x2
req df3afe40 actual 0x400 length0x400 buf df53b400
req df3afde0 actual 0x400 length0x400 buf df53b800
req df3afb40 actual 0x400 length0x400 buf df53a000
req df3af540 actual 0x400 length0x400 buf df53b000
- for 3 packet/microframe:
root@freescale ~$ cat /proc/driver/fsl_usb2_udc
ARC USBOTG Device Controller driver
fsl-usb2-udc version: 1 August 2005
Gadget driver: g_webcam
USBCMD reg:
SetupTW: 0
Run/Stop: Run
USB Status Reg:
Dr Suspend: 0Reset Received: 0System Error: NormalUSB Error Interrupt: Err detected
USB Intrrupt Enable Reg:
Sleep Enable: 1SOF Received Enable: 0Reset Enable: 1
System Error Enable: 1Port Change Dectected Enable: 1
USB Error Intr Enable: 1USB Intr Enable: 1
USB Frame Index Reg:Frame Number is 0xb74
USB Device Address Reg:Device Addr is 0x1c000000
USB Endpoint List Address Reg:Device Addr is 0xcf391000
USB Port Status&Control Reg:
Port Transceiver Type : UTMIPort Speed: High Speed
PHY Low Power Suspend: Low power modePort Reset: Not in ResetPort Suspend Mode: Not in
Over-current Change: NoPort Enable/Disable Change: Not change
Port Enabled/Disabled: EnableCurrent Connect Status: Attached
USB Mode Reg:Controller Mode is : Device Controller
Endpoint Setup Status Reg:SETUP on ep 0x0
EP Ctrl Reg [0x0]: = [0x800080]
EP Ctrl Reg [0x1]: = [0x0]
EP Ctrl Reg [0x2]: = [0x840000]
EP Ctrl Reg [0x3]: = [0x0]
EP Ctrl Reg [0x4]: = [0x0]
EP Ctrl Reg [0x5]: = [0x0]
EP Ctrl Reg [0x6]: = [0x0]
EP Ctrl Reg [0x7]: = [0x0]
EP Prime Reg = [0x0]
For ep0 Maxpkt is 0x40 index is 0x0
req df584f60 actual 0x1a length 0x1a buf df4826c0
For ep2in Maxpkt is 0x400 index is 0x2
req df3faf00 actual 0x400 length0x400 buf df58a000
req df3fac00 actual 0x400 length0x400 buf df58b000
req df3fab40 actual 0x400 length0x400 buf df58b400
req df3fae40 actual 0x400 length0x400 buf df58b800
"mult" (in arcotg_udc.c) is directly related to the number of packets/microframe, but for me it's use looks good.
The only problem I've found is in "fsl_ep_queue()" function; "udc" is declared and then used with no initialization. This issue is solved moving the line "udc = ep->udc;" to the beginning of the function. Unfortunately, this looks no to be related with the issue I'm experiencing.
I don't know how to continue. Please, any advice is welcome.
Gonzalo.
Joan Carles, I don't think so:
in 0x0c00 bits[12-11]= 01 so 1 aditional packet (total of 2 packets/uframe)
in 0x1400 bits[12-11]= 10 so 2 additional packets (total of 3 packets/uframe)
Dooty, I'll work on this after Easter. If documentation is accurate and there is no (undocumented) silicon bug, most of the work is done. Anyway, I'm using a mainline kernel, and things are a bit different than in FSL BSP. If needed, I expect to find support in the USB mailing list.
Regards,
Gonzalo.
Hi Gonzalo,
Thank you for your reply. Without freescale support, have you tried to implement high bandwidth isochronous support in UVC gadget driver. What is the current status?. Is it possible to develop UVC gadget driver for high bandwidth Isochoronus support without help of freescale.
Regards,
Dooty.
I'm sorry to say I didn't find a solution. The answer from Freescale to my Technical Service Request was that this feature was not supported.
On the other hand, I also need a solution for this problem, but on a iMX25. I've just started to investigate this issue on a 3.2.2 kernel but I have some preliminary problems (the USB engine is constantly reseting when plugged to a PC and still don't know if this is a harware/software problem). As I'm currently busy in another project, I'll come back to this issue after Easter, and will report my findings here.
Regards,
Gonzalo