i.MX53QSB BSP and kernel source not available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53QSB BSP and kernel source not available

1,090 Views
199694
Contributor I

Regarding the i.MX53QSB, all links to BSP releases and documentation are dead.

Please advise on where to obtain BSP source code, documentation, U-Booot source code, and the imx_2.6.35_maintain branch of git://git.freescale.com/imx/linux-2.6-imx.git for kernel source

References:

https://community.nxp.com/t5/i-MX-Processors/where-to-get-Freescale-L2-6-35-11-05-01-ER-source-bundl...

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX53-QSB-Board-Get-Started/ta-p/112498...

0 Kudos
Reply
5 Replies

1,057 Views
199694
Contributor I

@Rita_Wang Thank you for the link, all the linked files are downloaded.

However, there is an issue with powerup hangs. Turns out a further set of patches to L2.6.35_11_09_ER_SOURCE was needed to enhance reliability. Would you have these update files as per the refenced article (2)?

IMX53_LINUX_1109_BSP_PATCH, IMX53_1109_LINUX_MMDOCS, IMX53_11_09_LINUX_MMCODECS, AACP_CODECS_LINUX_11_09

References

(1)

https://community.nxp.com/t5/i-MX-Processors/iMX53-QSB-Powerup-Hangs/m-p/206865?tstart=0

(2)

https://community.nxp.com/t5/i-MX-Processors/New-Linux-11-09-BSP-Patch-for-the-i-MX53-blog-archive/m...

0 Kudos
Reply

1,087 Views
199694
Contributor I

@TomE if you are still around, I hope you can be of help as you've worked on this in the past!

Tags (1)
0 Kudos
Reply

1,085 Views
TomE
Specialist II

I asked Google and it found this post, saying everything has moved to github:

https://community.nxp.com/t5/i-MX-Processors/git-freescale-com-down/m-p/996004

But read the whole of the above. It complains they only moved ONE repo to github and that 93 repos (and/or branches) are missing.

That happened 14 months ago.

That also shows the danger of relying on "remote repositories" in builds. You should always have local mirrors of everything.

Tom

 

0 Kudos
Reply

1,081 Views
199694
Contributor I

Hi Tom, thanks so much for your reply. It is sad that nothing can be done.

I got a bare i.MX53QSB and I'd hate to trash the board over the lack of documentation and source.

Perhaps someone from NXP can help as this stuff must surely be archived internally.

Please ping me if anyone has a copy of the L2.6.35_11.09.01_ER_source_bundle.tar.gz

Referenced from: https://boundarydevices.com/revisiting-ltib-and-qt-on-i-mx51-and-i-mx53/

 

 

0 Kudos
Reply

1,072 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I can share to you by the baidu pan

link: https://pan.baidu.com/s/1Pi30ma5FTpogYMW0eZA-zQ password: wk93

0 Kudos
Reply