Hi,
Have custom hardware is based on i.MX535 Sabre platform.
The primary display connected is TFT LCD, while the secondary display connected is Component TV-Out.
The custom BSP is based on the Android R10.4 release.
The following links were referred & applied the patches specified for "DUAL_VIDEO_SIN_UI"
(a) https://community.freescale.com/docs/DOC-94879
(b) https://community.freescale.com/thread/306934
(c) https://community.freescale.com/thread/307006
The video is seen on the TV, but it is with a green background. Do we need to make any other configurations? Is there any settings to be done with respect to the color conversion mapping? Pls advice.
The following are the configurations done:
1.bootargs
setenv bootargs 'console=ttymxc0 init=/init root=/dev/mmcblk1p2 rootfstype=ext4 rootwait di0_primary pmem=32M,64M fbmem=10M gpu_memory=32M video=mxcdi0fb:YUV444,TV-PAL tve'
2.init.rc
SECOND_DISPLAY_ENABLED 1
3.init.freescale.rc
setprop rw.SIN_VIDEO_DUAL_UI 0
setprop rw.DUAL_VIDEO_SIN_UI 1
setprop rw.secfb.disable-overlay 1
4.ueventd.rc
/sys/devices/platform/mxc_sdc_fb.0/graphics/fb* fsl_disp_property 0660 system graphics
/sys/devices/platform/mxc_sdc_fb.1/graphics/fb* fsl_disp_property 0660 system graphics
/sys/devices/platform/mxc_sdc_fb.0/graphics/fb* mode 0660 system graphics
/sys/devices/platform/mxc_sdc_fb.1/graphics/fb* mode 0660 system graphics
Regards,
Sridevi
解決済! 解決策の投稿を見る。
Qiang_FSL Apr 24, 2014 1:56 AM (in response to jamesbone)
Please reference to attached patches.
We are already reviewing your question, internally we will provide an answer
Qiang_FSL Apr 24, 2014 1:56 AM (in response to jamesbone)
Please reference to attached patches.
Hi,
Unable to access the files specified. Pls share.
Regards,
Sridevi
Let me add you the patch.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Jaime,
As per your advice i have applied patches for r10.4, and configured as below in init.rc.
setprop rw.SIN_VIDEO_DUAL_UI 0setprop rw.DUAL_VIDEO_SIN_UI 1setprop rw.secfb.disable-overlay 1
But , still i am unable to play video on secondary display which is my Tvout. so please tell me where i am doing wrong to play video on dual displays .
Thanx in advance ,
suman.