Hi,
which is the best linux kernel version to use as start point for a custom design based on an imx53 quickstart board?
The article Linux Kernel is a good information source, and http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git
seems to be the right repository. But which branch should be used? Thanks in advance.
已解决! 转到解答。
That is the right repository. You can also use the Kernel mainline, but I am not sure which things are not supported. In case you want this (to use the latest), install Yocto, select your machine and follow this document https://community.freescale.com/docs/DOC-94971
Leo
That is the right repository. You can also use the Kernel mainline, but I am not sure which things are not supported. In case you want this (to use the latest), install Yocto, select your machine and follow this document https://community.freescale.com/docs/DOC-94971
Leo