i.MX53 nand partition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 nand partition

ソリューションへジャンプ
1,424件の閲覧回数
chengwu
Contributor I

Dear all,

     I'm developing a wince7 BSP on an i.MX53 board, my system could boot up from nand flash now, and I could use remote tools to attach to my board, now I need to store some files into the file system when the OS is running, and the files should not lose when the system is power down, that means I should write the files into nand flash directly, so how can I do this? I know that I should mount the user partition of nand flash as a disk when the system boot up, and write my files into the disk, but I don't know how to do that, can anybody help me? Thank you very much.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,288件の閲覧回数
Yuri
NXP Employee
NXP Employee

You may use the "Storage Manager to format and create partitions on the

mounted NAND device". Please refer to Chapter 20 (NAND Flash Driver)

of "WCE700_MX53_ER_1105_SMD_ReferenceManual.pdf".

http://cache.freescale.com/files/32bit/doc/support_info/WCE700_MX53_ER_1105_SMD_DOCKIT.zip

In particular : section 20.6.1 (System Testing)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,289件の閲覧回数
Yuri
NXP Employee
NXP Employee

You may use the "Storage Manager to format and create partitions on the

mounted NAND device". Please refer to Chapter 20 (NAND Flash Driver)

of "WCE700_MX53_ER_1105_SMD_ReferenceManual.pdf".

http://cache.freescale.com/files/32bit/doc/support_info/WCE700_MX53_ER_1105_SMD_DOCKIT.zip

In particular : section 20.6.1 (System Testing)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信