i.MX53 gstreamer on framebuffer?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 gstreamer on framebuffer?

9,180 Views
sidebranch
Contributor II

Are there examples on how to use the gstreamer codec plugins on the i.MX53 without X Windows running on the target?

Has someone played decoded video to the framebuffer?

Thanks,

Leon.

Labels (1)
Tags (2)
0 Kudos
Reply
17 Replies

4,546 Views
sidebranch
Contributor II

Yes it seems you are right that _MX51 must be defined. However, the configure user message suggests otherwise:

configure.ac:251:  AC_MSG_ERROR(No target platform specified! Use ./configure PLATFORM=(MX28/MX233/MX25/MX27/MX31/MX35/MX37/MX51/MX53/MX50/MX5X/MX6) to retry)

If specifying PLATFORM=MX53 this will define _MX53 as a preprocessor symbol during compilation. However, there is no check for _MX53, only for MX51 and smaller platforms.

So I think MX53/MX50/MX5X/MX6 will fail (and possible are Freescale internal new developments).

Thanks Kan HU, this fixed my problem.

0 Kudos
Reply

4,546 Views
KanHU
Contributor III

You maybe simply comment these sentences to see what happened. 

maybe the some macro is not defined, it should defined _MX51

0 Kudos
Reply

4,546 Views
sidebranch
Contributor II

If I disable this piece of code, the decoding suddenly works:

if (v4l_info->buffers_required > max_frames) {
            v4l_info->buffers_required = max_frames;
        }

I wonder why I need this change in my build, as nobody else seems to have this problem.

Regards,

Leon.

0 Kudos
Reply

4,546 Views
sidebranch
Contributor II

I have continued my analysis why no video is played out from my build:

In the "gst-fsl-plugin-2.0.3.tar.gz" package, the source file "mfw_gst_v4lsink.c" and the function "mfw_gst_v4lsink_buffer_alloc()":

        max_frames = MAX_V4L_ALLOW_SIZE_IN_BYTE / frame_buffer_size;

        if (v4l_info->buffers_required > max_frames) {
            v4l_info->buffers_required = max_frames;
        }

resulted in v4l_info->buffers_required = 2.

which resulted in mfw_gst_v4l.c: mfw_gst_v4l2_output_setup() to not allocate any buffers at all; this loop condition was never true:

    while (v4l_info->buffers_required >= MIN_BUFFER_NUM) {

    }

I have added extra Gstreamer debugging prints to demonstrate what happens. I do not have a clue yet why the Ubuntu provided image behaves differently. Unfortunately I am running into LTIB problems I have to solve, as that would provide a third basis.

0:00:01.058964251  1231    0xf39c0 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:1890:mfw_gst_v4lsink_buffer_alloc: Decoded Width = 1920, Decoded Height = 1088
0:00:01.059034001  1231    0xf39c0 WARN             mfw_v4lsink mfw_gst_v4lsink.c:1213:mfw_gst_v4lsink_set_format: set to nv12 mode
0:00:01.059086376  1231    0xf39c0 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:1902:mfw_gst_v4lsink_buffer_alloc: Decoder maximal reserved 12 buffers.
0:00:01.059323751  1231    0xf39c0 INFO             mfw_v4lsink mfw_gst_v4lsink.c:1933:mfw_gst_v4lsink_buffer_alloc: MAX_V4L_ALLOW_SIZE_IN_BYTE / frame_buffer_size = max_frames (7340032 / 3133440 = 2)
0:00:01.059380376  1231    0xf39c0 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:1936:mfw_gst_v4lsink_buffer_alloc: Decoder maximal support 2 buffers.
0:00:01.059429626  1231    0xf39c0 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:1940:mfw_gst_v4lsink_buffer_alloc: v4l_info->buffers_required reduced to max_frames = 2
0:00:01.059703626  1231    0xf39c0 INFO             mfw_v4lsink mfw_gst_v4l.c:1007:mfw_gst_v4l2_set_fmt: mfw_gst_v4l2_set_fmt()
0:00:01.059797751  1231    0xf39c0 INFO             mfw_v4lsink mfw_gst_v4l.c:1137:mfw_gst_v4l2_set_fmt: v4l_info->buffers_required = 2
0:00:01.059887126  1231    0xf39c0 INFO             mfw_v4lsink mfw_gst_v4l.c:942:mfw_gst_v4l2_output_setup: v4l_info->buffers_required = 2
0:00:01.059941126  1231    0xf39c0 INFO             mfw_v4lsink mfw_gst_v4l.c:943:mfw_gst_v4l2_output_setup: MIN_BUFFER_NUM = 5
0:00:01.059990126  1231    0xf39c0 INFO             mfw_v4lsink mfw_gst_v4l.c:974:mfw_gst_v4l2_output_setup: v4l_info->swbuffer_max = 0
0:00:01.060038751  1231    0xf39c0 ERROR            mfw_v4lsink mfw_gst_v4l.c:1141:mfw_gst_v4l2_set_fmt: Error in mfw_gst_v4lsink_output_setup

0 Kudos
Reply

4,546 Views
sidebranch
Contributor II

I have included the log for that.

I think it goes wrong at this point, I just cannot figure out why yet. The full log is in the attachment.

0:00:03.544888354  1233    0xd2fc0 ERROR            mfw_v4lsink mfw_gst_v4l.c:1130:mfw_gst_v4l2_set_fmt: Error in mfw_gst_v4lsink_output_setup
>>V4L_SINK: Actually buffer status:
    hardware buffer : 0
    software buffer : 0
0:00:03.545144729  1233    0xd2fc0 ERROR            mfw_v4lsink mfw_gst_v4l_buffer.c:630:mfw_gst_v4l2_buffer_init: Failed to allocate buffer pool container
0:00:03.545243854  1233    0xd2fc0 WARN             mfw_v4lsink mfw_gst_v4l_buffer.c:400:mfw_gst_v4l2_new_buffer: Try new buffer failed, ret 2 No such file or directory queued 0
0:00:03.545417854  1233    0xd2fc0 DEBUG            mfw_v4lsink mfw_gst_v4l_buffer.c:404:mfw_gst_v4l2_new_buffer: Finally assign a sw buffer from queue, left:0.
0:00:03.575604104  1233    0xd2fc0 DEBUG            mfw_v4lsink mfw_gst_v4l_buffer.c:69:mfw_gst_v4lsink_buffer_finalize: Buffer 0 maybe dropped.

0 Kudos
Reply

4,546 Views
KanHU
Contributor III

could you try "export GST_DEBUG=mfw_vpudecoder:4,mfw_v4lsink:4,GST_CAPS:4", 

I need more information for analysis. 

0 Kudos
Reply

4,546 Views
sidebranch
Contributor II

No this is independent of Linaro. We are working on the Yocto Project and the OpenEmbedded Core.

This is mainly voluntary work by me in the community as I need this for a project, whilst Alonso Lazcano Adrian (B38018) is working to get Freescale teams to work on mainlining.

Freescale has already taken over my work for PowerPC mainlining in Yocto.

We can re-use the Linaro work. We mostly work on the build infrastructure for Yocto, not necessarely on kernel/user space fixes.

However I do want to verify that what I check in and bring up stream actually works.

0 Kudos
Reply

4,546 Views
sidebranch
Contributor II

Sorry the log was not complete. I've deleted the old log and attached the new log instead.

0 Kudos
Reply

4,546 Views
KanHU
Contributor III

really strange, like the vpu did not set good caps to v4lsink

 

btw, I'm wondering which team you are with for upstream to which project? linaro?  

0 Kudos
Reply

4,546 Views
sidebranch
Contributor II

Thank you for looking along. I build from the meta-freescale repository at GitHub, this is for OpenEmbedded.  I know this is not LTIB, but I am working with the Freescale team to bring this upstream. This should match the 11.09.01 source code release.

Attached is the log for

export GST_DEBUG=mfw_vpudecoder:4,GST_CAPS:4

time gst-launch filesrc location=/trailer_1080p.mov ! qtdemux ! mfw_vpudecoder ! mfw_v4lsink

0 Kudos
Reply

4,546 Views
KanHU
Contributor III

where you build from? 

 

can you post log with "export GST_DEBUG=mfw_vpudecoder:4,GST_CAPS:4"

0 Kudos
Reply

4,546 Views
sidebranch
Contributor II

My own build gives "hardware buffer : 0" and gives no codec video output to the screen.

The Ubuntu SD card gives "hardware buffer : 12" and works.

What can be the reason for this difference?

I have built and executed the alpha tool just to be sure it is no alpha/colorkey issue.

0 Kudos
Reply

4,546 Views
KanHU
Contributor III

v4l sink is default output to fb2

composite for fb0 and fb2 is controlled by alpha value or colorkey 

there's ioctl for alpha setting 

struct mxcfb_gbl_alpha g_alpha; 

fd = open("/dev/fb0", O_RDWR, 0);

g_alpha.alpha = 128;
g_alpha.enable = 1;
ioctl(fd, MXCFB_SET_GBL_ALPHA, done, &g_alpha);

the alpha is from 0 to 255.

 

the hardware buffer number is for internal debug only, you can ignore the information. 

0 Kudos
Reply

4,546 Views
WolfgangW
Contributor I

Sorry, I didn't find out where to set transparency either.

Trying with gst-launch, my output looks mostly similar:

root@freescale ~$ gst-launch filesrc location=/mnt/cdrom/hd_other_samsung_led_motion.m2ts ! ffdemux_mpegts ! mfw_vpudecoder ! mfw_v4lsink
MFW_GST_V4LSINK_PLUGIN 2.0.3 build on Nov 25 2011 23:46:26.
Setting pipeline to PAUSED ...
[INFO] Product Info: i.MX53
VPU Version: firmware 13.4.41; libvpu: 5.3.2
MFW_GST_VPU_DECODER_PLUGIN 2.0.3 build on Nov 25 2011 23:45:31.
Pipeline is PREROLLING ...
>>V4L_SINK: Actually buffer status:
hardware buffer : 11
software buffer : 0
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
full screen size:1920x1080
[V4L Update Display]: left=0, top=0, width=1920, height=1080
New clock: GstSystemClock
video4linux video16: Bypassing IC
mxc_ipu mxc_ipu: Channel already disabled 10
mxc_ipu mxc_ipu: Channel already uninitialized 10
mxc_ipu mxc_ipu: Channel already disabled 10
mxc_ipu mxc_ipu: Channel already uninitialized 10
VPU blocking: timeout.
VPU blocking: timeout.
...

I am not sure if the number of hardware buffers at this point is meaningful? And, in my case, there is the message " video4linux video16: Bypassing IC" - what is IC? Might be image combiner...?

BTW, this is a full HD video you're playing... Did you see and follow this post?

0 Kudos
Reply

4,546 Views
sidebranch
Contributor II

Thank you. To answer your last question first: Yes, this is exactly what I mean with framebuffer playout. I was unsure if the V4L2 output used the fb device.

I have tested the following on the supplied Ubuntu SD image:

time gst-launch filesrc location=/trailer_1080p.mov ! qtdemux ! mfw_vpudecoder ! mfw_v4lsink

I see the video play correctly in the background, even when I kill the X Windows server at the same time. This is OK.

In my self-built image, I think I have an issue with the transparency, but opposite to your situation, in my case the framebuffer remains visible, but the video is invisible.

Where can this transparency be set?

MFW_GST_V4LSINK_PLUGIN  build on Dec 14 2011 13:56:30.
Setting pipeline to PAUSED ...
[INFO]    Product Info: i.MX53
VPU Version: firmware 13.4.41; libvpu: 5.3.2
MFW_GST_VPU_DECODER_PLUGIN  build on Dec 14 2011 13:56:16.
Pipeline is PREROLLING ...
>>V4L_SINK: Actually buffer status:
    hardware buffer : 0
    software buffer : 0
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
full screen size:1024x768
[V4L Update Display]: left=0, top=0, width=1024, height=768
New clock: GstSystemClock
Got EOS from element "pipeline0".
Execution ended after 32461977000 ns.
Setting pipeline to PAUSED ...
total time:0:00:32.480843375 ,Render fps:0
Setting pipeline to READY ...
Setting pipeline to NULL ...
Total rendered:0

>>VPU_DEC: State: Ready to Null
Freeing pipeline ...
[--->FINALIZE vpu_dec

0 Kudos
Reply

4,546 Views
WolfgangW
Contributor I

Short update:

Playback on raw framebuffer (actually: overlay via v4l) works with gst-launch as well as gplay in the same way.

With my self-compiled filesystem image, the overlay is also used without transparency, so the framebuffer contents is not visible while playing video - I remember this was different with the original Freescale image.

However, on second reading I am not sure if this is what you mean by "played decoded video to the framebuffer"?

0 Kudos
Reply

4,546 Views
WolfgangW
Contributor I

Hi Leon,

I only tried with gplay lately, but this one works flawlessly without any X running. Have to check with gst-launch tomorrow, but AFAIR it also worked without X. Only thing is that I did not yet figure out how to set up overlay correctly (blinking cursor of the framebuffer visible on the video...)

Best regards,

Wolfgang 

0 Kudos
Reply