I have a i.MX53 board which is currently being used with a VGA display. I want to set it up to use a LVDS1 display instead.
According to the quick start guide we are supposed to enable the LVDS output using U-Boot. Is U-Boot already installed along with the Ubuntu that comes with the 4 GB Micro SD card or do I have to install it myself?
解決済! 解決策の投稿を見る。
Hi Jill,
U-boot is already installed on SD card. Yes, to change the booting arguments, you need
to connect PC to the board with the serial cable (RS-232).
I think it is already set up to output through LVDS.
You need to modify the booting arguments to send the output to LVDS instead of VGA.
Please take a look at the user guide to modify the arguments to use LVDS (attached)
Best regards,
Sergio
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for your reply.
I've already read the user guide. My doubt is whether I'll have to install U-Boot myself or if it is already preinstalled on the provided micro SD card (which contains Linux).
I'm asking this because I have limited access to the board. If I have to install U-Boot I'd like to know beforehand so that I can be prepared for it. If it's already installed and I only have to change the booting arguments then that's easy. An additional question, to change the booting arguments do I need to connect to the board using the serial cable (RS-232)?
Hi Jill,
U-boot is already installed on SD card. Yes, to change the booting arguments, you need
to connect PC to the board with the serial cable (RS-232).
Hi,
Do you know if it is possible to change the U-Boot variables without the serial cable (RS-232)? For example, directly from the Ubuntu that comes pre-installed on the SD card.
Thanks!
I don't think it is possible.
What is the issue on getting a serial cable? ;-)
Oh, my computer doesn't even have a serial port! :smileyconfused:
Mine doesn't as well. You can get a USB to serial adapter :-)
Good idea, thank you!