i.MX53 accidentally fell into security mode at boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 accidentally fell into security mode at boot

862 Views
torus1000
Contributor V

Hi,

One of i.MX53 sometimes accidentally fell into security mode(SM=01) after boot up in spite of other i.MX53 always keep on SM=00,  I don't know why.

Why did SM bit change to 01 and SRTC LP alarm? Which condition assumed to cause this issue?

Is there any workaround?

Here is SRTC register difference:

   reg     normal     issue happened

   ------- ---------- -----------

  LPSCMR  0x6        0x0        //LPSC mid

  LPSCLR  0xc80000   0x0        //LPSC low

  LPSAR   0x0        0x0

  LPSMCR  0x0        0x0

  LPCR    0xc008     0xc000     //EN_LP

  LPSR    0xe008     0xe400    //Security Mode(SM)=01,Alarm Flag of LP section*1

  LPPDR   0x41736166 0x41736166

   ------- ---------- -----------

*1: Indicates that the SRTC LP secured counter alarm has occurred.

Can anyone help me?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

751 Views
art
NXP Employee
NXP Employee

The most likely cause of the issue is the effect of the silicon erratum ENGcm12374, please refer to its description in the i.MX53 Chip Errata Rev.6 document, available on the processor's Documentation web page:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply