Now we are trying to display WSXGA+(1680x1050) on LVDS LCD in Ubuntu,
using our custom board based on i.MX53 QSB-R.
LVDS configuration is as follows.
- One dual channel output: single input, split to two output channels
Most resolution (UXGA/1080p etc) except WSXGA+ can be displayed.
However, WSXGA+(1680x1050) can be displayed without "xserver-xorg-video-imx".
Are there any hardware or software limitations?
Additional information:
- Using the display driver : [xserver-xorg-video-imx_11.09.01_armel.deb] (latest)
-> To display WSXGA+(1680x1050) on LVDS LCD is failure.
- Using the display driver : [xserver-xorg-video-imx_11.03.00-1_armel.deb]
-> To display WSXGA+(1680x1050) on LVDS LCD is success, but video playback is failure.
Does anybody know how to display WSXGA+ on LVDS LCD and do video playback
with the latest "xserver-xorg-video-imx"?