i.MX53 Sabre Tablet Audio Path Setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 Sabre Tablet Audio Path Setup

643 Views
ChuckFarago
Contributor I

How do I set up the LINEIN to I2S to i.MX53 to Bluetooth audio path on the i.MX53 Sabre tablet?

Labels (1)
0 Kudos
1 Reply

490 Views
Yuri
NXP Employee
NXP Employee

If the Bluetooth configuration is alredy working ou only need the following:

1) Be sure in your Bluetooth firmware the audio output is set to PCM line or I2S.

2) Configure in your board file ( in case of Linux)  the proper I2S line to be used.

3) Maybe you need to add some pull up on the line.

0 Kudos