i.MX53 SD card I/F usage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX53 SD card I/F usage

跳至解决方案
1,457 次查看
ko-hey
Senior Contributor II

Hi all

I want to confirm about the meaning of the word "Pull up" in Table 30-1 at following document.

http://cache.freescale.com/files/32bit/doc/ref_manual/iMX53RM.pdf?

In the Table 30-1, there is a column that named "Pull up".

What is this mean ?

Does the user should be pull up for each signals ?

However, in the schematics of SABRE Platform for Tablets Reference Design based on i.MX53, the SD1_DATA0, SD1_DATA1 and SD1_DATA2 signals are not pull-uped.

Because of those difference, I'm confusing.

So please let me know the meaning of the column.

pastedImage_1.png

Ko-hey

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,401 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

yes pull-ups are needed, SD1_DATA have internal pull-ups,

if necessary external pull-ups may be added for improving signal integrity.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,402 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

yes pull-ups are needed, SD1_DATA have internal pull-ups,

if necessary external pull-ups may be added for improving signal integrity.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,401 次查看
ko-hey
Senior Contributor II

Igor

Thanks!

Ko-hey

0 项奖励
回复