i.MX53 SABRE Tablet - "failed to run command" error from MfgTool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 SABRE Tablet - "failed to run command" error from MfgTool

772件の閲覧回数
dn
Contributor I

I am getting the following error from the MfgTool:

 

failed to run command: type="find" body="Updater" file="" timeout="180" onError="" text="" ,, Error code:-65530.

 

I get this error after receiving "Jumping to OS Image".

 

I am trying to flash an Android image to the i.MX53 SABRE Tablet.

 

Is there a workaround or a fix?

タグ(1)
0 件の賞賛
返信
1 返信

560件の閲覧回数
dn
Contributor I

I think I figured out my problem.  I modified player.ini by setting UCL_INSTALL_SECTION to equal MX53SMD-SD, replacing MX53EVK-SD, and ran MfgTool.  I got past my problem.

 

I think player.ini has to be modified so that UCL_INSTALL_SECTION points to the right LIST name in the ucl.xml file.

0 件の賞賛
返信