i.MX53 SABRE Tablet - "failed to run command" error from MfgTool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 SABRE Tablet - "failed to run command" error from MfgTool

1,507 Views
dn
Contributor I

I am getting the following error from the MfgTool:

 

failed to run command: type="find" body="Updater" file="" timeout="180" onError="" text="" ,, Error code:-65530.

 

I get this error after receiving "Jumping to OS Image".

 

I am trying to flash an Android image to the i.MX53 SABRE Tablet.

 

Is there a workaround or a fix?

Tags (1)
0 Kudos
Reply
1 Reply

1,295 Views
dn
Contributor I

I think I figured out my problem.  I modified player.ini by setting UCL_INSTALL_SECTION to equal MX53SMD-SD, replacing MX53EVK-SD, and ran MfgTool.  I got past my problem.

 

I think player.ini has to be modified so that UCL_INSTALL_SECTION points to the right LIST name in the ucl.xml file.

0 Kudos
Reply