i.MX53 Reference Manual Errors, is there a list?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX53 Reference Manual Errors, is there a list?

2,011 次查看
TomE
Specialist II

I'm going through the Reference Manual and finding a lot of obvious errors (apart from the spelling errors).

There doesn't seem to be an Errata or update to this manual.

Is anyone keeping a list of errors, because Freescale doesn't seem to be doing this.

Is there a "place" of some sort on this site where this sort of document could be created, indexed and more importantly FOUND by others using this manual?

Here are ones I've found in the following document over the course of a few days trying to track down a DDR3 memory problem that happens at high and low temperatures.

i.MX53 Multimedia Applications Processor Reference Manual

Document Number: iMX53RM

Rev. 2.1, 06/2012

Table 43-2. DDR Output Driver Average Impedance

    DDR3 mode - Calibration resistance = 200

    This doesn't match:

    43.3.454 IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE

        NVCC_EMI_DRAM=1.5V+/-5% (DDR3), ddr_sel='00': 240 Ohm

Table 43-2. DDR Output Driver Average Impedance

    DDR3 mode: Hi-Z4, 240, 120, 80, 60, 48, 48, 34.

    The resistance values listed for "5" and "6" are the same.

    I have measured the resistances on the DDR_RESET pin as

    approximately "246, 108, 71, 53, 43, 35, 30" indicating

    that the duplicates in the table are a a mistake. The

    equivalent tables in the i.MX6 manuals give 240, 120,

    80, 60, 48, 40 and 34 ohms.

43.3.343 IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS3

43.3.347 IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS2

43.3.352 IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS0

43.3.357 IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS1

    Both the Diagram and Table state that the 22:24 field is

    "Reserved and Read Only" when it has to be written with

    the ODT value, as these pins are I/O (as are the data pins).

    Checking the registers in the debugger shows these bits to be

    read/write and the Freescale sample code sets these bits.

    The Diagram also shows the Reset state as "1" wuile the

    Description shows it as "0".

43.3.353 IOMUXC_SW_PAD_CTL_PAD_DRAM_SDODT0

43.3.346 IOMUXC_SW_PAD_CTL_PAD_DRAM_SDODT1

    The SDODT0 register diagram has the ODT field read/write whereas

    the description has it read-only, and the register is read-only.

    The SDODT1 section is correct.

43.3.344 IOMUXC_SW_PAD_CTL_PAD_DRAM_SDCKE1

43.3.356 IOMUXC_SW_PAD_CTL_PAD_DRAM_SDCKE0

    The register diagram has the DSE field read/write whereas the

    description has it read-only, and the register is read-only.

43.3.359 IOMUXC_SW_PAD_CTL_PAD_PMIC_ON_REQ

43.3.360 IOMUXC_SW_PAD_CTL_PAD_PMIC_STBY_REQ

    The Register Diagram gives the Reset State of the DSE_TEST and PUE

    bits as "1" while the description has them as "0". The "Strength Mode"

    bit is the reverse,"0" in the Diagram and "1" in the Description.

43.3.358 IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM1

    The Diagram shows the PUE reset value of "1" and the PUS reset

    value of "00" whereas the text shows PUS as "0" and PUS as "10".

    The DQM0, DQM2 and DQM3 sections are correct.

43.3.278 IOMUXC_SW_PAD_CTL_PAD_JTAG_TDO

    The Diagram gives DSE and SRE as read-only while the Description

    has them as read-write.

43.3.351 IOMUXC_SW_PAD_CTL_PAD_DRAM_SDCLK_0

    The Diagram gives PKE, PUE and PUS as read-write whereas the

    Description has them as read-only. The SDCLK_1 section is OK.

In Addemdum 2:

Table 2-10. Common Fusemap

    Address 0C00 is shown to be in Bank 0 when it is in Bank 1. This

    is correct in section 2.2.

2.2 Fusemap Description Table

    Addresses 1814, 1818 and 181C are shown to be in Bank 0. This

    is correct in Table 2-10.

Tom

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

1,614 次查看
gusarambula
NXP TechSupport
NXP TechSupport

It is true that documentation can sometimes hold  several errors and Freescale does work on updating documentation constantly. As you see the Reference Manual is now on revision 2.1 and there is still work to be done!

I’m double checking and escalating these observations so they are considered for the next revision of the document. Please note that it might take some time for changes to be reflected on a new release.

There is no central repository for this feedback as it’s intended to be finally reflected on the official document but your input in our communities will very likely serve other users to be aware of these errors and we’re taking notes on them.

Thank you for taking the time to documenting these errors and pointing them out!

0 项奖励
回复

1,614 次查看
TomE
Specialist II

> I’m double checking and escalating these observations so they are considered for the next revision of the document.

Thank you for that.

> Freescale does work on updating documentation constantly.

But this manual is so old (June 2012) that from previous experience I wasn't expecting any further revisions or addenda.

> There is no central repository for this feedback

Freescale use to have a Ticket System for this, but that has been closed down.

Do you have any idea why these manuals have these spelling errors in them? A run over with a spelling checker should be easy to do. Maybe you have a "company technical dictionary" and these mis-spellings have accidentally been added to it, that's happened before. The number of obvious spelling errors lowers confidence in the technical content when all these have slipped through the checking. I listed a few of them here:

i.MX53 & i.MX6 Reference Manual Spelling Problems

My favourites are "CSU manges system sucurity alarms", "writting, wrotten, wrutten", "regitsers, regitsters, regsier, regsiter, regsiters", "cannnot" and most ironically, "accruate".

Tom

0 项奖励
回复