i.MX53 Quick Start Board (Ltib Or Yacto)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 Quick Start Board (Ltib Or Yacto)

Jump to solution
2,051 Views
vidyasagartata
Contributor II

Dear All,

Could any one provide specific link for the download ths LTIB or yacto for i.MX53 quick start board.

For software development which one is easy either ltib or yacto.

Also suggest me host configuration for ubuntu 12.04 LTS.

Thanks,

Vidya

Labels (1)
0 Kudos
Reply
1 Solution
1,668 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vidya

below link for latest ltib BSP:

Linux 2.6.35 Source Code Files and documentation 11.09. Supports MCIMX53-START and MCIMX53-START-R (REV 2011.09)

GZ (1.1 GB) L2.6.35_11_09_ER_SOURCE

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab

https://community.freescale.com/docs/DOC-95042  ubuntu configurations

yocto links :

https://lists.yoctoproject.org/pipermail/meta-freescale/2014-July/009102.html

https://community.freescale.com/thread/331977

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
1,669 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vidya

below link for latest ltib BSP:

Linux 2.6.35 Source Code Files and documentation 11.09. Supports MCIMX53-START and MCIMX53-START-R (REV 2011.09)

GZ (1.1 GB) L2.6.35_11_09_ER_SOURCE

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab

https://community.freescale.com/docs/DOC-95042  ubuntu configurations

yocto links :

https://lists.yoctoproject.org/pipermail/meta-freescale/2014-July/009102.html

https://community.freescale.com/thread/331977

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,668 Views
vidyasagartata
Contributor II

Dear Igor,

I am following below link :

i.MX53 Quick Start - Linux on ARM - eewiki

and got compiled the u-boot.

Please let me know how to boot the i.mx53 quick start board.

What boot need to follow for the MMC boot, is it possible to flash the MMC card through MFG tool.

Please specified some user guide or link to do boot the i.mx53 quick start board.

We are planning to design custom board based on the i.mx7, please help me brief in this regard and how we will get the evaluation kit based on i.mx7.

Thanks,

Vidya

0 Kudos
Reply
1,668 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vidya

please look at attached Linux Guide.

Regarding i.MX7, since it is not released yet

please contact local FAE for its availability.

Best regards

igor

0 Kudos
Reply
1,668 Views
vidyasagartata
Contributor II

Dear Igor,

I am trying to load images in the micro sd card through MFG tool as followed by 3.1 steps in i.MX53_START_Linux_BSP_UserGuide.pdf , gets fails and gives error

Updater Error 0xffff0000 (-65536) -

also connected the serial console in minicom but u-boot log does not show.

Please let me know why images are not getting flash in the micro sd card.

Thanks,

Vidya

0 Kudos
Reply
1,668 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vidya

please create new thread for this problem

and provide full name and web links of used image

and mfg tools. It is recommended to start with :

Recommended Software & Tools (1)

Linux Binary Demo Files 11.09 Release (REV 2011.09)

Linux Binary Demo Files 11.09 Release.

Programmers (Flash, etc.) (3)

IMX_MFG_TOOL (REV 1.6.2.048)

Tool and documentation for downloading OS images to the i.MX53, i.MX51, i.MX50, i.MX28 and i.MX23.

ZIP (247.0 MB) IMX_MFG_TOOL

i.MX53 Quick Start Board|Freescale

Best regards

igor

0 Kudos
Reply