i.MX53 QSB and 10 wire CMOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 QSB and 10 wire CMOS

Jump to solution
980 Views
andrzejnowak
Contributor I

Hi,

first of all I would like to introduce myself as it is my first post here.

My name is Andrzej and we are slowly starting new project in Poland.

I would like to make sure about one detail regarding QSB:

Is there any chance to connect through the expansion port a CMOS sensor that requires 10 data wires (10bit)?

My idea was to build daughterboard that would contain camera module connected to CSI0 data, v&h sync, reset, clock lines (pins) and I2S1 or I2S2 port. But according to the "Hardware User Guide for i.MX53 Quick Start Board, Preliminary Rev 0.9" table 27 "Expansion Port Pin-Mux Table (con)" there are only 8 pins for CSI0 data available (that would be CSI0_DAT12 : CSI0_DAT19).

Is there any way to use other pins for CSI0_DAT10 and CSI0_DAT11?

I will appreciate any opinion from you!


best regards
Andrzej

Labels (1)
0 Kudos
1 Solution
748 Views
BrilliantovKiri
Senior Contributor I

Hello, Andrzej!

Unfortunally QSB have only 8 CSI0 lines on expand slot, you can examine this http://cache.freescale.com/files/32bit/doc/ref_manual/IMX53RQSBRM-R.pdf?fpsp=1&WT_TYPE=Reference%20M...

View solution in original post

0 Kudos
3 Replies
749 Views
BrilliantovKiri
Senior Contributor I

Hello, Andrzej!

Unfortunally QSB have only 8 CSI0 lines on expand slot, you can examine this http://cache.freescale.com/files/32bit/doc/ref_manual/IMX53RQSBRM-R.pdf?fpsp=1&WT_TYPE=Reference%20M...

0 Kudos
748 Views
andrzejnowak
Contributor I

Thanks Kirill.

I just wanted to make sure and now i have no doubts.

Cheers

0 Kudos
748 Views
aksispd
Contributor II

Technically there are a lot of empty pins on the expansion header, you can jumper the UART1 TX and RX line (logic level) and change the debug port to UARTn.

0 Kudos