i.MX53 GPT(Geeral Purpose Timer).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 GPT(Geeral Purpose Timer).

847 Views
mujeebshaik
Contributor II

Hi,

I am new to i.MX53

i am using i.MX53 QSB board OS:WinCE700

i want count the Pulses/Second which are given in on one GPIO pin externally,

i am planning to use the GPT(General Purpose Timer) Module.by that we can capture the external pulses as per datasheet.

so if any one have idea on this how to use GPT Module,if any one knows please give me the suggestion so that it will be helpfull to me.

Thansk & Regards,

Shaik.

Labels (2)
0 Kudos
2 Replies

543 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

According to the Release note document GPT driver is not supported in the Wince MX53 SMD BSP. However Please check the i.Mx51 EVK BSP GPT driver under

Third Party > BSP > Freescale <Target Platform>: ARMV4I > Device Drivers > Timers >General-purpose Timer Support

Regards

0 Kudos

543 Views
mujeebshaik
Contributor II


Hi Bio_TICFSL,

Thanks for your reply,

In iMX53 QSB Board the driver is available,Third Party -> Freescale i.MX53 QSB:ARMV7 -> Device Drivers -> Timers -> General-purpose Timer Support

Please share the example to access from applicaion.

Thanks

Shaik

0 Kudos