i.MX53 Embedded-Qt-4.7.0 touchscreen wrong points positions and events

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX53 Embedded-Qt-4.7.0 touchscreen wrong points positions and events

986 次查看
leroy_o
Contributor III

I am using a Sabre platform for i.MX53 with a LVDS1 LCD / touchpanel, with tslib.

When using Embedded-Qt-4.7.0 applications that make use of the cursor position, when I tap on the screen, sometimes, the cursor moves at a location distant from the point where I tap. Also there are two mouse events mouseButtonpressed, instead of one when the application behaves correctly in this case.

Recalibrating the touchscreen doesn't solve the problem.

This problem occurs only on Embedded-Qt-4.7.0 applications. The output of "hexdump /dev/input/event0" is correct. So this is not a low level issue.

Have someone experienced the same with Embedded-Qt applications, and solved it?

标签 (3)
0 项奖励
回复
0 回复数