i.MX53 DDR3 stress test - Not working for correct configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 DDR3 stress test - Not working for correct configuration

1,741 Views
KeshavaGN
Contributor V

Hi all,

I am trying DDR stress test application by freescale on imx53.

I have custom board with following specs:

1GHz processor freq

400 GHz DDR freq

2 DDR3 chips with 128 MB each (total 256MB)

Previously I tried DDR stress test with input as:

1 DDR3 chip of 256 MB. In which DDR stress test is running fine.

But later I changed this to actual configuration (that is : 2 DDR

chips of 128 MB each) in which DDR stress test is failing.

Please help me to understand the problem.

Is there any particular changes needed in code/.inc file?

Thanks.

With regards,

Keshava

Labels (1)
0 Kudos
Reply
6 Replies

1,191 Views
Yuri
NXP Employee
NXP Employee

You wrote about using two configurations :

- "1 DDR3 chip of 256 MB" ;

- "2 DDR chips of 128 MB each".

Please let me look at connection schematic of both cases.

0 Kudos
Reply

1,191 Views
yanglius
Contributor I

Hello.  i am runing IMX536 With Mircon DDR3 MT41K256M16 ¨C 32 Meg x 16 x 8 banks DDR3 test. i download the inc file(the inc file name is MX53_TO2_DDR3_LCB_SMD_ARDb) from FSL.so i just modify the TRFC.TXS and some Parameters. run ddr test. the calibration is success. but the DDR test is fail. could you tell me whrer need to modify?

// Enable CSD0 and CSD1, row width = 15, column width = 10, burst length = 8, data width = 32bit

setmem /32 0x63fd9000 = 0xc3190000 //Main control register

// tRFC=208ck;tXS=68;tXP=3;tXPDLL=10;tFAW=24;CAS=4ck

setmem /32 0x63fd900C = 0x9f5152e3 //timing configuration Reg 0.

// tRCD=11;tRP=11;tRC=39;tRAS=28;tRPA=1;tWR=15;tMRD=4;tCWL=6ck

setmem /32 0x63fd9010 = 0xb68e8a63 //timing configuration Reg 1

// tDLLK(tXSRD)=512 cycles; tRTP=4;tWTR=4;tRRD=4

setmem /32 0x63fd9014 = 0x01ff00db //timing configuration Reg 2

setmem /32 0x63fd902c = 0x000026d2 //command delay (default)

setmem /32 0x63fd9030 = 0x009f0e21 //out of reset delays

// Keep tAOFPD, tAONPD, tANPD, and tAXPD as default since they are bigger than calc values

setmem /32 0x63fd9008 = 0x12273030 //ODT timings

// tCKE=5; tCKSRX=5; tCKSRE=5

setmem /32 0x63fd9004 = 0x0002002d //Power down control

0 Kudos
Reply

1,191 Views
KeshavaGN
Contributor V

Hi Yuri ,

Thanks for quick reply.

Actually we have only one hardware configuration. That is: "2 DDR chips of 128 MB each".

But due to misunderstanding, Initially, I used wrong input, i.e.: "1 DDR3 chip of 256 MB", for which stress test is working fine.

But, now it is not working for actual configuration, i.e.: "2 DDR chips of 128 MB each".

As of now, I don't have schematic, as it is customer board.

But customer confirmed that it is "2 DDR chips of 128 MB each".

Thanks again.

Regards,

Keshava

1,191 Views
Yuri
NXP Employee
NXP Employee

I just would like to know how two DDR chips are connected to i.MX53 - if both i.MX53 DDR CSs are used (one per DDR) or DDRs are connected
to the same CS (in parallel, 2 x 16 bit) ?

0 Kudos
Reply

1,191 Views
KeshavaGN
Contributor V

Hi Yuri,

Thanks for reply.

I asked with hardware team and it is confirmed that same CS is connected to both the DDRs.

Please advice...

Thanks & regards,

Keshava

From: Yuri Muhin

Sent: Wednesday, May 28, 2014 1:24 PM

To: Keshava G N

Subject: Re: - i.MX53 DDR3 stress test - Not working for correct configuration

i.MX53 DDR3 stress test - Not working for correct configuration

reply from Yuri Muhin in i.MX Community - View the full discussion

1,191 Views
Yuri
NXP Employee
NXP Employee

So, looks like, data port size has been changed between the two configurations :

- "1 DDR3 chip of 256 MB" ;

- "2 DDR chips of 128 MB each".

As result memory initialization should differ in port size. Is it so ?

0 Kudos
Reply