i.MX53 DDR Memory Controller and SPD EEPROM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 DDR Memory Controller and SPD EEPROM

Jump to solution
1,863 Views
sherry_zahid
Contributor III

Hello,

I am using an iMX535 with two micron DDR3 modules (MT41K512M16HA). My question is related to the memory controller on the iMX53. 

Does the iMX535 memory controller have the ability to read / implement the settings stored in the SPD (serial presence detect) EEPROM on the DDR3 module?  

Thanks,

Labels (1)
0 Kudos
Reply
1 Solution
1,723 Views
igorpadykov
NXP Employee
NXP Employee

Hi sherry

>Does the iMX535 memory controller have the ability to read / implement the settings

>stored in the SPD (serial presence detect) EEPROM on the DDR3 module?  

unfortunately not, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,724 Views
igorpadykov
NXP Employee
NXP Employee

Hi sherry

>Does the iMX535 memory controller have the ability to read / implement the settings

>stored in the SPD (serial presence detect) EEPROM on the DDR3 module?  

unfortunately not, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,723 Views
sherry_zahid
Contributor III

Thanks Igor

0 Kudos
Reply