i.MX51 SBMR - e-Fuses & GPIO overrides

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX51 SBMR - e-Fuses & GPIO overrides

879 Views
BojanMerela
Contributor I

Hi,

 

We try to boot i.MX51 from NAND flash, but we have some difficulties...

 

1. All e-Fuses are intact (not burned)

2. We use GPIO pins to override e-Fuses (GPIO_BT_SEL = intact)

3. But not all GPIO pins are sampled to SBMR, just some...

4. For example we can set BT_MEM_TYPE to: 01 and it reflects in SBMR, but setting this to: 10 shows up as 00 in SBMR, on the iMX51 EVK board we see the same result

5. We are reading SBMR using ATK (custom nand kernel image). BMODE=00 and BMODE=10

6. If we program some binary to flash than we will not get to the serial downloader

 

any clues?

 

best regards,

Bojan

Tags (1)
0 Kudos
Reply
1 Reply

743 Views
BojanMerela
Contributor I
never mind... it was a stupid software bug...
0 Kudos
Reply