Hello,
I'm configuring NOR Flash as boot device by looking at Table 6-9 in RM below.
Does this instruct that, for NOR Flash boot, the Flash pins must be connected to the Pads specified in this table?
Then ROM code configures the IOMUXes the Pads without setting correspondent GPIO pins?
Does this sentence mean that we need to the configure shadowed pins by GPIO to be assingned propery to the specified Pad at reset?
However we don't need to configure manually for non-shadowed pins because ROM code does that.
We only need to conigure shadowed pins by GPIO.
Is this correct?
Best regards,
Nori Shinozaki
已解决! 转到解答。
Hi Nori
yes it is correct, for NOR Flash boot the flash pins must be connected to
the pads specified in this table. Also non-shadowed pins are
set by ROM code, no need to additionally configure them.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Igor,
Now please explain how to configure shadowed EIM_D[0] to EPDC_D0.ALT2 as shown in the table when it's reset for NOR boot.
When I look at the IOMUXC register for EPDC_D0, the default value for MUX_MODE is 0001(GPIO[0]).
How can I set 010 for EIM_D[0]?
Also I have to set the SELECT_INPUT register to mode ALT2.
How can I do that?
Best regards,
Nori Shinozaki
Nori,
there is no need for configuration of EIM_D[0] EPDC_D0.ALT2
since NOR boot is performed on D16-D31 pads (selection
BOOT_CFG2[7:6]=01 - Not Muxed, 16-bit data (high half) interface)
EIM_DA0-15.ALT0 are for selection BOOT_CFG2[7:6]=00 - Muxed, 16-bit data (low half) interface
Shadowed pads are not used for boot.
Best regards
igor
Hello Igor,
Thanks again,
Let me confirm the Table 23-2 below
Is these correction in red are correct?
Because...
BOOT_CFG2[7:6]=00 - Muxed, 16-bit data (low half:DA0-15) interface
From 23.101.1 EIM_CSGCR1,
MUM=1
DSZ=001(lower 2bits applied)
So EIM_BOOT=0x101
BOOT_CFG2[7:6]=01 - Not Muxed, 16-bit data (high half:D16-31) interface
From 23.101.1 EIM_CSGCR1,
MUM=0
DSZ=010(lower 2bits applied)
So EIM_BOOT=0x010
Best regards,
Nori Shinozaki
Hello Nori,
it is not necessary to use 23.101.1 EIM_CSGCR1
since iROM changes these settings as described in i.MX50 RM Boot Chapter:
NOR boot is performed on D16-D31 pads (selection
BOOT_CFG2[7:6]=01 - Not Muxed, 16-bit data (high half) interface)
EIM_DA0-15.ALT0 are for selection BOOT_CFG2[7:6]=00 - Muxed, 16-bit data (low half) interface
Shadowed pads are not used for boot. This corresponds to:
EIM_CS0GCR1[MUM] = ~BOOT_CFG2[6];
DSZ[0] = EIM_CS0GCR1[16] = ~ (BOOT_CFG2[7] | BOOT_CFG2[6]);
~igor
Hello Igor,
Thank you!
You mean DSZ[1] isn't cared, right?
Then, EIM_BOOT can be either of following values.
#Not muxed: BOOT_CFG2[7:6] = 0x01
EIM_BOOT[2:0] = 0x000
2: MUM = 0
1:DSZ[1] = *(say, 0)
0:DSZ[0] = 0
#Muxed: BOOT_CFG2[7:6] = 0x00
EIM_BOOT[2:0] = 0x101
2: MUM = 1
1: DSZ[1] = *(say, 0)
0: DSZ[0] = 1
So, as long as we use Not Muxed, 16-bit data (high half) settings, we don't neet to care about the 23.101.1 EIM_CSGCR1 register. Because ROM will set it so.
In other words, we can use Muxed mode by settings EIM_BOOT[2:0] pins in 0x101.
Best regards,
Nori Shinozaki
Hello Nori,
yes, ROM sets EIM_CSGCR1 register
BOOT_CFG2[7:6]=00 - Muxed, 16-bit data (low half) interface => DSZ = 001
BOOT_CFG2[7:6]=01 - Not Muxed, 16-bit data (high half) interface) =>DSZ = 010
DSZ[1] =~ (~(BOOT_CFG2[7] ^ BOOT_CFG2[6]);
~igor
Hello Igor,
Thanks but you wanted to write
DSZ[1] =~ (~BOOT_CFG2[7] ^ BOOT_CFG2[6]);
?
Now it tuned out my customer has to use D0-15 pins to connect NOR FLASH for booting.
They need to set BOOT_CFG2[7:6]=00 by GPIO Boot Overrides as written in the Table 6-8 below
Then when I look at Table 6-3 to try to find out the GPIO pins but there are no "Contact" for BOOT_CFG2[7:6].
How can we really set BOOT_CFG2[7:6]=00?
BTW, EIM_BOOT[2:0] are internal signals generated by BOOT_CFG2[7:6]?
Best regards,
Nori Shinozaki